请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ76952 您好!
我将使用 BQ76952和 Stm32L431控制器、
我有一些疑问、
- 如何读取具有特定 CC3电流、CC1电流 CC2计数、CC3计数以及这些字节引用的值的数据状态0x0075寄存器。
- 我们为什么要将字节移位8、16、32、虽然这样做、但无法获得确切的电流值。
在这里、我附上了我 的 C 代码供参考、
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>
Copyright (c) 2021 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include<stdio.h>
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define DEV_ADDR 0x10 // Device address
#define CRC_Mode 0 // 0 for disabled, 1 for enabled
#define MAX_BUFFER_SIZE 10 //Max buffer size
//#define DEBUG_RX_DO_Pin GPIO_PIN_10
//#define DEBUG_RX_DO_GPIO_Port GPIOA
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
TIM_HandleTypeDef htim1;
TIM_HandleTypeDef htim2;
UART_HandleTypeDef huart1;
/* USER CODE BEGIN PV */
uint8_t spiData [2];
uint8_t spiRxData [2];
uint8_t rxdata [2];
uint8_t busyData [2] = {0xFF, 0xFF};
uint8_t TX_2Byte [2] = {0x00, 0x00};
uint8_t TX_3Byte [3] = {0x00, 0x00, 0x00};
uint8_t TX_4Byte [4] = {0x00, 0x00, 0x00, 0x00};
uint8_t TX_6Byte [6] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t TX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
uint8_t RX_2Byte [2] = {0x00, 0x00};
uint8_t RX_3Byte [3] = {0x00, 0x00, 0x00};
uint8_t RX_4Byte [4] = {0x00, 0x00, 0x00, 0x00};
uint8_t RX_6Byte [6] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t RX_12Byte [12] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t RX_32Byte [32] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,0x00,0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,0x00 ,0x00, 0x00, 0x00, 0x00,0x00, 0x00};
uint8_t RX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
unsigned int RX_CRC_Check = 0;
// Variables for cell voltages, temperatures, CC2 current, Stack voltage, PACK Pin voltage, LD Pin voltage
uint16_t CellVoltage [16] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
float Temperature [3] = {0,0,0};
float FET_Temperature = 0;
float HDQ_Temp = 0;
float DCHG_Temp = 0;
float DDSG_Temp = 0;
uint16_t Stack_Voltage = 0x00;
uint16_t LD_Voltage = 0x00;
uint16_t PACK_Voltage = 0x00;
uint16_t PACK_Current = 0x00;
float Current = 0;
uint16_t AlarmBits = 0x00;
uint32_t Samp1[2] ={0x00, 0x00};
uint32_t Res = 0;
uint32_t Min_cell = 0;
uint32_t Max_cell = 0;
uint32_t CC3_Current;
uint32_t CC1_Current;
uint32_t Raw_CC2_Count;
uint32_t Raw_CC3_Count;
uint8_t SafetyStatusA; // Safety Status Register A
uint8_t SafetyStatusB; // Safety Status Register B
uint8_t SafetyStatusC; // Safety Status Register C
uint8_t PFStatusA; // Permanent Fail Status Register A
uint8_t PFStatusB; // Permanent Fail Status Register B
uint8_t PFStatusC; // Permanent Fail Status Register C
uint8_t FET_Status; // FET Status register contents See TRM Section 12.2.20 - Shows states of FETs
uint16_t CB_ActiveCells; // Cell Balancing Active Cells
uint16_t DEVICE_NUMBER;
uint8_t UV_Fault = 0; // under-voltage fault state
uint8_t OV_Fault = 0; // over-voltage fault state
uint8_t SCD_Fault = 0; // short-circuit fault state
uint8_t OCD_Fault = 0; // over-current fault state
uint8_t LD_ON = 0; // Load Detect status bit
uint8_t DCHG = 0; // discharge FET state
uint8_t CHG = 0; // charge FET state
uint8_t PCHG = 0; // pre-charge FET state
uint8_t PDSG = 0; // pre-discharge FET state
uint32_t AccumulatedCharge_Int;
uint32_t AccumulatedCharge_Frac;
uint32_t AccumulatedCharge_Time;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_TIM1_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_TIM2_Init(void);
/* USER CODE BEGIN PFP */
void delayUS(uint32_t us) { // Sets the delay in microseconds.
//uint8_t tim = 0;
__HAL_TIM_SET_COUNTER(&htim1,0); // set the counter value a 0
while (__HAL_TIM_GET_COUNTER(&htim1) < us);
}
void delay_ticks(uint32_t ticks)
{
SysTick->LOAD = ticks;
SysTick->VAL = 0;
SysTick->CTRL = SysTick_CTRL_ENABLE_Msk;
// COUNTFLAG is a bit that is set to 1 when counter reaches 0.
// It's automatically cleared when read.
while ((SysTick->CTRL & SysTick_CTRL_COUNTFLAG_Msk) == 0);
SysTick->CTRL = 0;
}
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
uint8_t copyIndex = 0;
for (copyIndex = 0; copyIndex < count; copyIndex++)
{
dest[copyIndex] = source[copyIndex];
}
}
unsigned char Checksum(unsigned char *ptr, unsigned char len)
// Calculates the checksum when writing to a RAM register. The checksum is the inverse of the sum of the bytes.
{
unsigned char i;
unsigned char checksum = 0;
for(i=0; i<len; i++)
checksum += ptr[i];
checksum = 0xff & ~checksum;
return(checksum);
}
unsigned char CRC8(unsigned char *ptr, unsigned char len)
{
unsigned char i;
unsigned char crc=0;
while(len--!=0)
{
for(i=0x80; i!=0; i/=2)
{
if((crc & 0x80) != 0)
{
crc *= 2;
crc ^= 0x107;
}
else
crc *= 2;
if((*ptr & i)!=0)
crc ^= 0x107;
}
ptr++;
}
return(crc);
}
void I2C_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
#if CRC_Mode
{
uint8_t crc_count = 0;
crc_count = count * 2;
uint8_t crc1stByteBuffer [3] = {0x10, reg_addr, reg_data[0]};
unsigned int j;
unsigned int i;
uint8_t temp_crc_buffer [3];
TX_Buffer[0] = reg_data[0];
TX_Buffer[1] = CRC8(crc1stByteBuffer,3);
j = 2;
for(i=1; i<count; i++)
{
TX_Buffer[j] = reg_data[i];
j = j + 1;
temp_crc_buffer[0] = reg_data[i];
TX_Buffer[j] = CRC8(temp_crc_buffer,1);
j = j + 1;
}
HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, TX_Buffer, count, 1000);
}
#endif
#if CRC_Mode < 1
HAL_StatusTypeDef state = HAL_OK;
state=HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
if(state != HAL_OK)
{
}
#endif
}
int I2C_ReadReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
unsigned int RX_CRC_Fail = 0; // reset to 0. If in CRC Mode and CRC fails, this will be incremented.
#if CRC_Mode
{
uint8_t crc_count = 0;
uint8_t ReceiveBuffer [10] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
crc_count = count * 2;
unsigned int j;
unsigned int i;
unsigned char CRCc = 0;
uint8_t temp_crc_buffer [3];
HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, ReceiveBuffer, crc_count, 1000);
uint8_t crc1stByteBuffer [4] = {0x10, reg_addr, 0x11, ReceiveBuffer[0]};
CRCc = CRC8(crc1stByteBuffer,4);
if (CRCc != ReceiveBuffer[1])
RX_CRC_Fail += 1;
RX_Buffer[0] = ReceiveBuffer[0];
j = 2;
for (i=1; i<count; i++)
{
RX_Buffer[i] = ReceiveBuffer[j];
temp_crc_buffer[0] = ReceiveBuffer[j];
j = j + 1;
CRCc = CRC8(temp_crc_buffer,1);
if (CRCc != ReceiveBuffer[j])
RX_CRC_Fail += 1;
j = j + 1;
}
CopyArray(RX_Buffer, reg_data, crc_count);
}
#endif
#if CRC_Mode < 1
// HAL_StatusTypeDef state = HAL_OK;
HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
//if(state != HAL_OK)
//{
//}
#endif
return 0;
}
void AFE_Reset() {
// Reset command. Resets all registers to default values or the values programmed in OTP.
TX_2Byte[0] = 0x12; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void AFE_Init() {
// Configures all parameters in device RAM
// Enter CONFIGUPDATE mode (Subcommand 0x0090) - It is required to be in CONFIG_UPDATE mode to program the device RAM settings
// See TRM Section 7.6 for full description of CONFIG_UPDATE mode
TX_2Byte[0] = 0x90; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
delayUS(2000);
// After entering CONFIG_UPDATE mode, RAM registers can be programmed. When programming RAM, checksum and length must also be
// programmed for the change to take effect. All of the RAM registers are described in detail in Chapter 13 of the BQ76952 TRM.
// An easier way to find the descriptions is in the BQStudio Data Memory screen. When you move the mouse over the register name,
// a full description of the register and the bits will pop up on the screen.
// A summary of the Data Memory is also in Section 13.9 of the TRM.
// 'Power Config' - Set DSLP_LDO - 0x9234 = 0x2D82 (See TRM section 13.3.2)
// Setting the DSLP_LDO bit allows the LDOs to remain active when the device goes into Deep Sleep mode
TX_4Byte[0] = 0x34; TX_4Byte[1] = 0x92; TX_4Byte[2] = 0x82; TX_4Byte[3] = 0x2D;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// 'REG0 Config' - set REG0_EN bit to enable pre-regulator
TX_3Byte[0] = 0x37; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x01;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// 'REG12 Config' - Enable REG1 with 3.3V output
TX_3Byte[0] = 0x36; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x0D;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// 'VCell Mode' - Enable 16 cells - 0x9304 = 0x0000 (See TRM section 13.3.2.19)
// 0x0000 sets the default value of 16 cells.
TX_4Byte[0] = 0x04; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0x00; TX_4Byte[3] = 0x00;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// 'Default Alarm Mask' - Enable FullScan and ADScan bits
// 0xF882
TX_4Byte[0] = 0x6D; TX_4Byte[1] = 0x92; TX_4Byte[2] = 0x82; TX_4Byte[3] = 0xF8;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// Enable protections in 'Enabled Protections A' 0x9261 = 0xBC (See TRM section 13.3.3.2)
// Enables SCD (short-circuit), OCD1 (over-current in discharge), OCC (over-current in charge),
// COV (over-voltage), CUV (under-voltage)
TX_3Byte[0] = 0x61; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x00; //0xFC
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// Enable all protections in 'Enabled Protections B' 0x9262 = 0xF7 (See TRM section 13.3.3.3)
// Enables OTF (over-temperature FET), OTINT (internal over-temperature), OTD (over-temperature in discharge),
// OTC (over-temperature in charge), UTINT (internal under-temperature), UTD (under-temperature in discharge), UTC (under-temperature in charge)
TX_3Byte[0] = 0x62; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x00; //0xF7
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
#if 1
// Set TS1 to measure Cell Temperature - 0x92FD = 0x07 (See TRM Section 13.3.2.12)
TX_3Byte[0] = 0xFD; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x07;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// Set TS3 to measure FET Temperature - 0x92FF = 0x0F (See TRM Section 13.3.2.14)
TX_3Byte[0] = 0xFF; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x0F;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
#endif
#if 1
// Set DFETOFF pin to control BOTH CHG and DSG FET - 0x92FB = 0x42 (set to 0x00 to disable)
// See TRM section 13.3.2.10, Table 13-7
#if 0
TX_3Byte[0] = 0xFB; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0xC2;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
#endif
// Set up Alert Pin - 0x92FC = 0x2A - See TRM Section 13.3.2.11, Table 13-8
// This configures the Alert pin to drive high (REG1 voltage) when enabled.
// Other options available include active-low, drive HiZ, drive using REG18 (1.8V), weak internal pull-up and pull-down
TX_3Byte[0] = 0xFC; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x2A;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
#endif
#if 1
// Set up Cell Balancing Configuration - 0x9335 = 0x03 - Automated balancing while in Relax or Charge modes
// See TRM Section 13.3.11. Chapter 10 of TRM describes Cell Balancing in detail
// Also see "Cell Balancing with BQ76952, BQ76942 Battery Monitors" document on ti.com
TX_3Byte[0] = 0x35; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x03;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// Set up COV (over-voltage) Threshold - 0x9278 = 0x55 (4301 mV)
// COV Threshold is this value multiplied by 50.6mV See TRM section 13.6.2
TX_3Byte[0] = 0x78; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x55;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// Set up SCD Threshold - 0x9286 = 0x05 (100 mV = 100A across 1mOhm sense resistor)
// See TRM section 13.6.7 0x05=100mV
TX_3Byte[0] = 0x86; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x05;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// Set up SCD Delay - 0x9287 = 0x03 (30 us) See TRM section 13.6.7
// Units of 15us
TX_3Byte[0] = 0x87; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x03;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// Set up SCDL Latch Limit to 1 to set SCD recovery only with load removal 0x9295 = 0x01
// If this is not set, then SCD will recover based on time (SCD Recovery Time parameter).
// See TRM section 13.6.11.1
TX_3Byte[0] = 0x95; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x01;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
#if 1
// precharge start V
TX_4Byte[0] = 0x0A; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0x48; TX_4Byte[3] = 0xF4;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// precharge stop V
TX_4Byte[0] = 0x0C; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0x1C; TX_4Byte[3] = 0xF3;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// precharge time out
TX_3Byte[0] = 0x0E; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x00;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//predischarge stop delta
TX_3Byte[0] = 0x0F; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x00;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//discharge current threshold
TX_4Byte[0] = 0x10; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0xE2; TX_4Byte[3] = 0xFF;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
// HAL_Delay(1);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//charge current threshold
TX_4Byte[0] = 0x12; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0xF6; TX_4Byte[3] = 0xFF;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
// HAL_Delay(1);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
#endif
// Maufcturing status init
TX_4Byte[0] = 0x43; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0x10; TX_4Byte[3] = 0x00;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
// HAL_Delay(1);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//Fet options
TX_3Byte[0] = 0x08; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x1F;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//Protection config
TX_4Byte[0] = 0x5F; TX_4Byte[1] = 0x92; TX_4Byte[2] = 0x00; TX_4Byte[3] = 0x00;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
// HAL_Delay(1);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//Discharg protection A
TX_3Byte[0] = 0x69; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x00;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//Discharg protection B
TX_3Byte[0] = 0x6A; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x00;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//Discharg protection C
TX_3Byte[0] = 0x6B; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x00;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//Body diode
TX_4Byte[0] = 0x73; TX_4Byte[1] = 0x92; TX_4Byte[2] = 0xEC; TX_4Byte[3] = 0xFF;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
// HAL_Delay(1);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//CC Gain
TX_6Byte[0] = 0xA8; TX_6Byte[1] = 0x91; TX_6Byte[2] = 0xF2; TX_6Byte[3] = 0x41; TX_6Byte[4] = 0x6F; TX_6Byte[5] = 0x41;
I2C_WriteReg(0x3E, TX_6Byte, 6);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_6Byte, 6); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//HDQ config
TX_3Byte[0] = 0x00; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x0B;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//DCHG thermistor config
TX_3Byte[0] = 0x01; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x0B;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//TS1 temp offset
TX_3Byte[0] = 0xCE; TX_3Byte[1] = 0x91; TX_3Byte[2] = 0x19;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//TS3 temp offset
TX_3Byte[0] = 0xD0; TX_3Byte[1] = 0x91; TX_3Byte[2] = 0x19;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//HDQ temp offset
TX_3Byte[0] = 0xD1; TX_3Byte[1] = 0x91; TX_3Byte[2] = 0x19;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//DCHG temp offset
TX_3Byte[0] = 0xD2; TX_3Byte[1] = 0x91; TX_3Byte[2] = 0x19;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
#if 0
//Data Status
TX_2Byte[0] = 0x76; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
delayUS(1000);
I2C_ReadReg(0x40, RX_12Byte, 12);
CC3_Current = (RX_12Byte[21]<<8) + (RX_12Byte[20]);
CC1_Current = (RX_12Byte[23]<<8) + (RX_12Byte[22]);
Raw_CC2_Count = ((RX_12Byte[27]<<24) + (RX_12Byte[26]<<16) + (RX_12Byte[25]<<8) + RX_12Byte[24]);
Raw_CC3_Count = ((RX_12Byte[31]<<24) + (RX_12Byte[30]<<16) + (RX_12Byte[29]<<8) + RX_12Byte[28]);
delayUS(1000);
#endif
#if 0
//TS3
TX_3Byte[0] = 0xFF; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x0B;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//TS1
TX_3Byte[0] = 0xFD; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x0B;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
#endif
#endif
#if 0
//******** Manufacturing Status******//
TX_4Byte[0] = 0x43; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0x50; TX_4Byte[3] = 0x00;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
// HAL_Delay(1);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x61, TX_2Byte, 2);
delayUS(1000);
//*********************************//
//******Fet options***************//
TX_3Byte[0] = 0x08; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x1F;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
//*********************************//
//**************All fets On*************//
TX_2Byte[0] = 0x96; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
delayUS(1000);
//***************************************//
AFE_ReadFETStatus();
#endif
// Exit CONFIGUPDATE mode - Subcommand 0x0092
TX_2Byte[0] = 0x92; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
delayUS(1000);
}
void Enable_REG1()
{
TX_2Byte[0] = 0x90; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
// 'REG0 Config' - set REG0_EN bit to enable pre-regulator
TX_3Byte[0] = 0x37; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x01;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// 'REG12 Config' - Enable REG1 with 3.3V output
TX_3Byte[0] = 0x36; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x0D;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
// Exit CONFIGUPDATE mode - Subcommand 0x0092
TX_2Byte[0] = 0x92; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
//delayUS(1000);
}
// ************************** Functions Written by Rohith********************//
void AFE_FETOptions(){
TX_3Byte[0] = 0x08; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x1F;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
}
void AFE_ManufacturingStatus(){
TX_4Byte[0] = 0x43; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0x50; TX_4Byte[3] = 0x00;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
// HAL_Delay(1);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x61, TX_2Byte, 2);
delayUS(1000);
}
void Manufacturing_Status_Read(){
}
void PDSG_TEST(){
TX_2Byte[0] = 0x1C; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void PCHG_TEST(){
TX_2Byte[0] = 0x1E; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void CHG_TEST(){
TX_2Byte[0] = 0x1F; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void DSG_TEST(){
TX_2Byte[0] = 0x20; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void Charge_Pump(){
TX_3Byte[0] = 0x09; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x01;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
delayUS(1000);
}
void Comm_Type(){
TX_3Byte[0] = 0x39; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x12;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
}
void Swap_Comm_Mode(){
TX_2Byte[0] = 0x90; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
TX_3Byte[0] = 0x39; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x12;
I2C_WriteReg(0x3E, TX_3Byte, 3);
//delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
TX_2Byte[0] = 0xBC; TX_2Byte[1] = 0x29;
I2C_WriteReg(0x3E,TX_2Byte,2);
TX_2Byte[0] = 0x92; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void Dfet_off(){
TX_3Byte[0] = 0xFB; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x00;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
}
void Cfet_off(){
TX_3Byte[0] = 0xFA; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x00;
I2C_WriteReg(0x3E, TX_3Byte, 3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
}
void Status_Read(){
uint8_t rd_data;
TX_2Byte[0] = 0x57; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
delayUS(2000);
I2C_ReadReg(0x40, RX_2Byte, 2);
rd_data = (RX_2Byte[1]*256 + RX_2Byte[0]);
}
void Vcell(){
TX_4Byte[0] = 0x04; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0x00; TX_4Byte[3] = 0x00;
I2C_WriteReg(0x3E, TX_4Byte, 4);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06; // Checksum and Length
I2C_WriteReg(0x60, TX_2Byte, 2);
}
//**************** End *************//
// ********************************* FET Control Commands ***************************************
void AFE_FET_ENABLE() {
// Toggles the FET_EN bit in the Manufacturing Status register. So this command can be used to enable or disable the FETs.
TX_2Byte[0] = 0x22; TX_2Byte[1] = 0x00; //0x22
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void AFE_FET_Control(uint8_t FET_states) { // Bit3 = PCHG_OFF, Bit 2 = CHG_OFF, Bit1 = PDSG_OFF, Bit 0 = DSG_OFF
TX_3Byte[0] = 0x97; TX_3Byte[1] = 0x00; TX_3Byte[2] = FET_states;
I2C_WriteReg(0x3E,TX_3Byte,3);
delayUS(1000);
TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
I2C_WriteReg(0x60, TX_2Byte, 2);
}
void DSG_PDSG_OFF() {
// Disable discharge (and pre-discharge) FETs
// Subcommand 0x0093 See TRM Table 5-8 (DSG_PDSG_OFF())
TX_2Byte[0] = 0x93; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void CHG_PCHG_OFF() {
// Disable charge (and pre-charge) FETs
// Subcommand 0x0094 See TRM Table 5-8 (CHG_PCHG_OFF())
TX_2Byte[0] = 0x94; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void AFE_ALL_FETS_OFF() {
// Disable all FETs with command 0x0095 See TRM Table 5-8
TX_2Byte[0] = 0x95; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void AFE_ALL_FETS_ON() {
// All all FETs to be enabled with command 0x0096 See TRM Table 5-8
TX_2Byte[0] = 0x96; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void AFE_BOTHOFF () {
// Disables all FETs using the DFETOFF (BOTHOFF) pin
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET); // DFETOFF pin (BOTHOFF) set low
}
void AFE_RESET_BOTHOFF () {
// Resets DFETOFF (BOTHOFF) pin
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET); // DFETOFF pin (BOTHOFF) set low
}
void AFE_ReadFETStatus() {
// Read FET Status to see which FETs are enabled
I2C_ReadReg(0x7F, RX_2Byte, 2);
FET_Status = (RX_2Byte[1]*256 + RX_2Byte[0]);
DCHG = 0x4 & RX_2Byte[0]; // discharge FET state
CHG = 0x1 & RX_2Byte[0]; // charge FET state
PCHG = 0x2 & RX_2Byte[0]; // pre-charge FET state
PDSG = 0x8 & RX_2Byte[0]; // pre-discharge FET state
}
// ********************************* End of FET Control Commands *********************************
// ********************************* AFE Cell Balancing Commands *****************************************
void CB_ACTIVE_CELLS() {
// Check status of which cells are balancing
TX_2Byte[0] = 0x83; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
I2C_ReadReg(0x40, RX_2Byte, 2);
CB_ActiveCells = (RX_2Byte[1]*256 + RX_2Byte[0]);
}
void CFET_OFF_LO(){
TX_2Byte[0] = 0x28; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E, TX_2Byte, 2);
}
void DFET_OFF_LO(){
TX_2Byte[0] = 0x28; TX_2Byte[1] = 0x01;
I2C_WriteReg(0x3E, TX_2Byte, 2);
}
// ********************************* End of AFE Cell Balancing Commands *****************************************
// ********************************* AFE Power Commands *****************************************
void AFE_DeepSleep() {
// Puts the device into DEEPSLEEP mode. See TRM section 7.4
TX_2Byte[0] = 0x0F; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void AFE_ExitDeepSleep() {
// Exits DEEPSLEEP mode. See TRM section 7.4
TX_2Byte[0] = 0x0E; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void AFE_ShutdownCommand() {
// Puts the device into SHUTDOWN mode. See TRM section 7.5
TX_2Byte[0] = 0x10; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void AFE_ShutdownPin() {
// Puts the device into SHUTDOWN mode using the RST_SHUT pin
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET); // Sets RST_SHUT pin
}
void AFE_ReleaseShutdownPin() {
// Releases the RST_SHUT pin
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET); // Resets RST_SHUT pin
}
void AFE_SLEEP_ENABLE() { // SLEEP_ENABLE 0x0099
// Allows the device to enter Sleep mode if current is below Sleep Current. See TRM section 7.3
TX_2Byte[0] = 0x99; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void AFE_SLEEP_DISABLE() { // SLEEP_DISABLE 0x009A
// Takes the device out of sleep mode. See TRM section 7.3
TX_2Byte[0] = 0x9A; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
// ********************************* End of AFE Power Commands *****************************************
// ********************************* AFE Status and Fault Commands *****************************************
uint16_t AFE_ReadAlarmStatus() {
// Read this register to find out why the Alert pin was asserted. See section 6.6 of the TRM for full description.
I2C_ReadReg(0x62, RX_2Byte, 2);
return (RX_2Byte[1]*256 + RX_2Byte[0]);
}
void AFE_ReadSafetyStatus() {
// Read Safety Status A/B/C and find which bits are set
// This shows which primary protections have been triggered
I2C_ReadReg(0x03, RX_2Byte, 2);
SafetyStatusA = (RX_2Byte[1]*256 + RX_2Byte[0]);
UV_Fault = 0x4 & RX_2Byte[0];
OV_Fault = 0x8 & RX_2Byte[0];
SCD_Fault = 0x8 & RX_2Byte[1];
OCD_Fault = 0x2 & RX_2Byte[1];
I2C_ReadReg(0x05, RX_2Byte, 2);
SafetyStatusB = (RX_2Byte[1]*256 + RX_2Byte[0]);
I2C_ReadReg(0x07, RX_2Byte, 2);
SafetyStatusC = (RX_2Byte[1]*256 + RX_2Byte[0]);
}
void AFE_ReadPFStatus() {
// Read Permanent Fail Status A/B/C and find which bits are set
// This shows which permanent failures have been triggered
I2C_ReadReg(0x0B, RX_2Byte, 2);
PFStatusA = (RX_2Byte[1]*256 + RX_2Byte[0]);
I2C_ReadReg(0x0D, RX_2Byte, 2);
PFStatusB = (RX_2Byte[1]*256 + RX_2Byte[0]);
I2C_ReadReg(0x0F, RX_2Byte, 2);
PFStatusC = (RX_2Byte[1]*256 + RX_2Byte[0]);
}
void AFE_ControlStatus() {
// Control status register - Bit0 - LD_ON (load detected)
// See TRM Table 6-1
I2C_ReadReg(0x00, RX_2Byte, 2);
LD_ON = 0x1 & RX_2Byte[0];
}
void AFE_BatteryStatus() {
// Battery status register - See TRM Table 6-2
I2C_ReadReg(0x12, RX_2Byte, 2);
}
void AFE_ClearFaults() {
TX_2Byte[0] = 0x00; TX_2Byte[1] = 0xF8;
I2C_WriteReg(0x62,TX_2Byte,2);
}
void AFE_ClearScanBits() {
TX_2Byte[0] = 0x82; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x62,TX_2Byte,2);
}
void AFE_PFReset() {
TX_2Byte[0] = 0x29; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
uint16_t AFE_DeviceID() {
// Read Device ID using Subcommand 0x0001
TX_2Byte[0] = 0x01; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
delayUS(500);
I2C_ReadReg(0x40, RX_2Byte, 2);
return (RX_2Byte[1]*256 + RX_2Byte[0]);
}
void AFE_STATUS(){
TX_2Byte[0] = 0x90; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
delayUS(1000);
TX_2Byte[0] = 0x75; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
delayUS(1000);
I2C_ReadReg(0x40, RX_32Byte, 32);
Max_cell = (RX_32Byte[5]<<8) + (RX_32Byte[4]);
Min_cell = (RX_32Byte[7]<<8) + (RX_32Byte[6]);
CC3_Current = (RX_32Byte[21]<<8) + (RX_32Byte[20]);
CC1_Current = (RX_32Byte[23]<<8) + (RX_32Byte[22]);
Raw_CC2_Count = ((RX_32Byte[27]<<24) + (RX_32Byte[26]<<16) + (RX_32Byte[25]<<8) + RX_32Byte[24]);
Raw_CC3_Count = ((RX_32Byte[31]<<24) + (RX_32Byte[30]<<16) + (RX_32Byte[29]<<8) + RX_32Byte[28]);
delayUS(1000);
TX_2Byte[0] = 0x92; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
// ********************************* End of AFE Status and Fault Commands *****************************************
// ********************************* AFE Measurement Commands *****************************************
uint16_t AFE_ReadCellVoltage(uint8_t channel) {
I2C_ReadReg(channel*2+0x14, RX_2Byte, 2);
return (RX_2Byte[1]*256 + RX_2Byte[0]); // cell voltage is reported in mV
}
uint16_t AFE_ReadStackVoltage() {
I2C_ReadReg(0x34, RX_2Byte, 2);
return 10 * (RX_2Byte[1]*256 + RX_2Byte[0]); // voltage is reported in 0.01V units
}
uint16_t AFE_ReadPackVoltage() {
I2C_ReadReg(0x36, RX_2Byte, 2);
return 10 * (RX_2Byte[1]*256 + RX_2Byte[0]); // voltage is reported in 0.01V units
}
uint16_t AFE_ReadLDVoltage() {
I2C_ReadReg(0x38, RX_2Byte, 2);
return 10 * (RX_2Byte[1]*256 + RX_2Byte[0]); // voltage is reported in 0.01V units
}
uint16_t AFE_ReadCurrent() {
//uint8_t cure = 0;
I2C_ReadReg(0x3A, RX_2Byte, 2);
return (RX_2Byte[1]*256 + RX_2Byte[0]); // current is reported in mA
}
float AFE_ReadTemperature(uint8_t channel) {
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_15, GPIO_PIN_SET);
switch(channel)
{
case 0:
I2C_ReadReg(0x70, RX_2Byte, 2); // TS1 pin
break;
case 1:
I2C_ReadReg(0x74, RX_2Byte, 2); // TS3 pin, FET temperature
break;
case 2:
I2C_ReadReg(0x76, RX_2Byte, 2); // HDQ, FET temperature
break;
case 3:
I2C_ReadReg(0x78, RX_2Byte, 2); // DCHG pin, FET temperature
break;
default: break;
}
return (0.1 * (float)(RX_2Byte[1]*256 + RX_2Byte[0])) - 273.15; // convert from 0.1K to Celcius
}
void AFE_ReadPassQ() {
// Read Accumulated Charge and Time from DASTATUS6 (See TRM Table 4-6)
TX_2Byte[0] = 0x76; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
delayUS(1000);
I2C_ReadReg(0x40, RX_12Byte, 12);
AccumulatedCharge_Int = ((RX_12Byte[3]<<24) + (RX_12Byte[2]<<16) + (RX_12Byte[1]<<8) + RX_12Byte[0]);
AccumulatedCharge_Frac = ((RX_12Byte[7]<<24) + (RX_12Byte[6]<<16) + (RX_12Byte[5]<<8) + RX_12Byte[4]);
AccumulatedCharge_Time = ((RX_12Byte[11]<<24) + (RX_12Byte[10]<<16) + (RX_12Byte[9]<<8) + RX_12Byte[8]);
}
void AFE_ClearPassQ() {
// Clear Accumulated Charge and Time, command 0x0082
TX_2Byte[0] = 0x82; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void config_mode(){
TX_2Byte[0] = 0x90; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
void Exit_config_mode(){
TX_2Byte[0] = 0x92; TX_2Byte[1] = 0x00;
I2C_WriteReg(0x3E,TX_2Byte,2);
}
// ********************************* End of AFE Measurement Commands *****************************************
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
volatile int i = 0;
char uart_buf[50];
int uart_buf_len;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_TIM1_Init();
MX_USART1_UART_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
//DFET PIN fetofff(low)
HAL_TIM_Base_Start(&htim1);
//HAL_GPIO_WritePin(GPIOC, GPIO_PIN_7, GPIO_PIN_RESET); // DEFET PIN
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_3, GPIO_PIN_RESET);
delayUS(10000);
AFE_Reset();
delayUS(60000);
AFE_Init();
delayUS(10000);
//AFE_FET_ENABLE();
//delayUS(10000);
AFE_ALL_FETS_ON();
AFE_ReadFETStatus();
delayUS(10000);
AFE_SLEEP_DISABLE();
delayUS(60000); delayUS(60000); delayUS(60000); delayUS(60000); //wait to start measurements after FETs close
CellVoltage[1] = AFE_ReadCellVoltage(1);
CellVoltage[5] = AFE_ReadCellVoltage(5);
CellVoltage[10] = AFE_ReadCellVoltage(10);
Stack_Voltage = AFE_ReadStackVoltage();
PACK_Voltage = AFE_ReadPackVoltage();
LD_Voltage = AFE_ReadLDVoltage();
//PACK_Current = AFE_ReadCurrent();
Temperature[0] = AFE_ReadTemperature(0);
FET_Temperature = AFE_ReadTemperature(1);
HDQ_Temp = AFE_ReadTemperature(2);
DCHG_Temp = AFE_ReadTemperature(3);
//DDSG_Temp = AFE_ReadTemperature(4);
// AFE_ALL_FETS_ON();
// AFE_ReadFETStatus();
#if 0
AFE_SLEEP_DISABLE();
AFE_ManufacturingStatus();
AFE_ReadFETStatus();
Charge_Pump();
AFE_FETOptions();
// AFE_FET_ENABLE();
AFE_FET_Control(0x00);
AFE_ReadFETStatus();
AFE_ALL_FETS_ON();
AFE_ReadFETStatus();
#endif
HAL_StatusTypeDef stat = HAL_OK;
stat = HAL_I2C_IsDeviceReady(&hi2c1,0x10,2,10);
if(stat == HAL_OK)
{
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
AFE_STATUS();
PACK_Current = AFE_ReadCurrent();
Current = PACK_Current * 14.9538;
AFE_ReadFETStatus();
// HAL_GPIO_WritePin(RS485_1_RO_DO_UC_GPIO_Port, UC_RDE_DO_RS485_1_Pin, 1); //Enable uart1
// HAL_GPIO_WritePin(UC_DI_DO_RS485_1_GPIO_Port, UC_RDE_DO_RS485_1_Pin, 1); // Enable UART1
// HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, 1); // Enable UART1
HAL_GPIO_WritePin(DEBUG_RX_DO_GPIO_Port, DEBUG_RDE_DO_Pin, 1);
for(int i = 0 ;i <=15; i++)
{
CellVoltage[i] = AFE_ReadCellVoltage(i);
printf("cell voltages [%d] = %d",i,CellVoltage);
}
Temperature[0] = AFE_ReadTemperature(0) * 10;
printf("Temperature ambient : %d",Temperature[0]);
FET_Temperature = AFE_ReadTemperature(1) * 10;
printf("Temperature Mosfet : %d",FET_Temperature);
HDQ_Temp = AFE_ReadTemperature(2) * 10;
printf("HDQ Temperature : %d",HDQ_Temp );
DCHG_Temp = AFE_ReadTemperature(3) * 10;
printf("DCHG Temperature : %d",DCHG_Temp );
// DDSG_Temp = AFE_ReadTemperature(4);
//pa10 port,pa8 pin,1
HAL_GPIO_WritePin(DEBUG_RX_DO_GPIO_Port, DEBUG_RDE_DO_Pin, 1);
// HAL_GPIO_WritePin(RS485_1_RO_DO_UC_GPIO_Port, UC_RDE_DO_RS485_1_Pin, 1); //Enable uart1
// HAL_GPIO_WritePin(RDE_DO_GPIO_Port, RDE_DO_Pin, 0); //Disable uart2
// HAL_GPIO_WritePin(GPIOA, GPIO_PIN_10, 1); // Enable UART1
// HAL_GPIO_WritePin(RS485_1_RO_DO_UC_GPIO_Port, UC_RDE_DO_RS485_1_Pin, 0); //Disable UART1
#if 1
if (AlarmBits & 0x82) {
AFE_ClearScanBits();
}
if (AlarmBits & 0xC000) {
AFE_ReadSafetyStatus();
AFE_ReadPFStatus();
AFE_ClearFaults();
AFE_PFReset();
}
#endif
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = 0;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 36;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_I2C1;
PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief I2C1 Initialization Function
* @param None
* @retval None
*/
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = 0x10808DD3;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/** Configure Analogue filter
*/
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
{
Error_Handler();
}
/** Configure Digital filter
*/
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
/**
* @brief TIM1 Initialization Function
* @param None
* @retval None
*/
static void MX_TIM1_Init(void)
{
/* USER CODE BEGIN TIM1_Init 0 */
/* USER CODE END TIM1_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM1_Init 1 */
/* USER CODE END TIM1_Init 1 */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 63;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 65535;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM1_Init 2 */
/* USER CODE END TIM1_Init 2 */
}
/**
* @brief TIM2 Initialization Function
* @param None
* @retval None
*/
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 63;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 65535;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OC_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_TIMING;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_4) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
/* USER CODE END TIM2_Init 2 */
}
/**
* @brief USART1 Initialization Function
* @param None
* @retval None
*/
static void MX_USART1_UART_Init(void)
{
/* USER CODE BEGIN USART1_Init 0 */
/* USER CODE END USART1_Init 0 */
/* USER CODE BEGIN USART1_Init 1 */
/* USER CODE END USART1_Init 1 */
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART1_Init 2 */
/* USER CODE END USART1_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(RST_SHUT_B_UC_GPIO_Port, RST_SHUT_B_UC_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(DFETOFF_B_UC_GPIO_Port, DFETOFF_B_UC_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, DEBUG_RDE_DO_Pin|UC_TEMP_EN_DO_M_Pin, GPIO_PIN_SET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(RDE_DO_GPIO_Port, RDE_DO_Pin, GPIO_PIN_RESET);
/*Configure GPIO pins : RST_SHUT_B_UC_Pin DEBUG_RDE_DO_Pin UC_TEMP_EN_DO_M_Pin */
GPIO_InitStruct.Pin = RST_SHUT_B_UC_Pin|DEBUG_RDE_DO_Pin|UC_TEMP_EN_DO_M_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : DFETOFF_B_UC_Pin */
GPIO_InitStruct.Pin = DFETOFF_B_UC_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(DFETOFF_B_UC_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : RDE_DO_Pin */
GPIO_InitStruct.Pin = RDE_DO_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(RDE_DO_GPIO_Port, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
请提供帮助、
谢谢、此致
罗希思西