This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 5V 输出电压中的纹波为300mV

Guru**** 2782445 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1030753/300mv-ripple-in-the-5v-output-voltage

器件型号:TPS54531

你(们)好

以下电路取自数据表第9.2节"典型应用"中的基准电路、根据是否有东西插入 USB 下行端口、我可以具有高达1A 的负载。

当我在内部接收到该电路并测试运行时、我在'+5V'节点上看到以下波形。

数据表中的图19。 Eco-mode 输出纹波看起来该纹波应该仅为20mV 左右。

是否有人可以帮助我了解我的输出电压纹波为何比数据表大得多?