请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:bq24600 bq24600不能正常工作、STAT 引脚闪烁、PG 低电平。但闪烁频率不是0.5Hz、直流电源电流重复显示0来设置充电电流(Viset 设置的充电值)跳转


设计中可能出错的原因?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
e2e.ti.com/.../db6a75a0e79cbe82be07e4c488e34e9d.mp4
直流电源的电流限值大于2A,电池电压约为12.3V。调试时、充电电流变为0.8A、而不是原理图上的值。如果电路受到干扰、为什么要定期呢? 太不可思议了。