您好的团队,
如果系统温度增加到90度,那么会发生什么情况?原因在数据表中,它写入了0-85度,我们可以启用充电。
我们是否可以充电?自动充电将关闭,或者,主机需要在过热时执行任何操作?
谢谢、
Smruti
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、
如果没有适配器、则仅负载和电池连接到 bq25713。电池已开始放电。我使用 bq studio 观察到这一点、然后突然出现 ACK 错误、我检查了电池电压、电压表中的0.001、锂离子电池2600mah、我观察到没有准确的电池电压 ADC 读数,有时电池电压为7V 时显示“ack error”(错误),有时显示为6伏。您能告诉我为什么没有特定的模式?
电池电压水平时,它应该会显示 ACK 错误。
谢谢、
Smruti