请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:BQ25730、 BQ24610大家好、
我们是否有单个 IC 解决方案可通过 30V/12A 直流电源在10A、1A、0.1A 和0.01A 范围内产生多个恒定电流? 20 微欧姆至2千欧姆范围内的预期负载。
提前感谢!
此致、
Jejomar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.