Other Parts Discussed in Thread: TPS51716
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS51716 请告诉我开关频率。
kΩ 数据表、在 Rmode = 12k Ω 时、工作频率为670kHz。 该"670 kHz"表示为典型值。
请告诉我负载电流为10A 时的最大和最小频率
请注意、
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.