请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:BQ35100大家好、
我们正在寻找适用于 LiFeS2的电池电量监测计、其要求如下、您能帮助提供价格合理的合适解决方案吗?
电池:一次性锂电池 S2、2S1P (3.6V~2V)
电流:10uA~5mA (睡眠)、10mA~2A (运行)
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.