您好!
我使用 LM317将5V 转换为3.6V (原理图如下所示)
当我在一段时间后将输入5V 设为0时、仍会在输出端获得1.5V 电压、该输出存在大约2-3秒、然后再变为0。 请告诉我它的原因以及使它变为0的方法

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好、Edgar

蓝色曲线:LM317输出
黄色曲线:LM317的输入
当电源关闭时、此时输入也不会变为0。 它在特定的持续时间内保持在1.25V、在此期间输出保持在1.04V。
我尝试在输出到输入之间放置一个二极管、这里的观察结果相同。
请告诉我如何将其设为0。
案例1:
输入电容:输入时为10uF 和0.1uF
输出电容:10uF
案例2:
输入电容:输入时为1uF 和0.1uF
输出电容:1uF
案例3:
输入电容: 输入时为0.1uF
输出电容:1uF
在所有这三种情况下、我都会得到类似的结果。
谢谢
Manish Sharma