请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS65287 各位专家,您好
我的客户有一个应用、可以生成接近0V 到高达12V 的可调电压。
1) 1)该器件可配置的最小和最大输出电压是多少?
2) 2)是否可以通过反馈路径中的 DAC 或可调电阻器来调节输出电压?
谢谢!
Jim B
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位专家,您好
我的客户有一个应用、可以生成接近0V 到高达12V 的可调电压。
1) 1)该器件可配置的最小和最大输出电压是多少?
2) 2)是否可以通过反馈路径中的 DAC 或可调电阻器来调节输出电压?
谢谢!
Jim B