请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ2980 主题中讨论的其他器件: BQ2970
您好!
您能否为单节电池推荐合适的保护 IC?
电池:LiFePO4、1节电池
OVP:3.7V~3.75V
电池工作范围:2V~3.65V
所需的高侧保护。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.