Other Parts Discussed in Thread: LM5156
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM5156尊敬的 TI 团队:
您能帮助我们为以下方面提供解决方案:
- 5V 至±18V @ 500mA
- 12V 至±40V @300mA
- 12V 至24V @ 500mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好 Sanjay、
请浏览此网站: 升压稳压器|德州仪器 TI.com
如果您按"查看所有产品"、您将看到我们所有升压转换器的列表、通过搜索、您可以找到适用于所有3种情况的合适器件。
此致、
Brigitte