请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24610 尊敬的 TI:
我对多节电池充电器 BQ24610有疑问。
如何平衡多节电池?
如果我将4.2V 和3.5V 的电池电压串联、它如何充电?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.