This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM5177:输出功率能力

Guru**** 2535750 points
Other Parts Discussed in Thread: LM5177

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1160914/lm5177-output-power-capabilities

器件型号:LM5177

各位专家:

我能不能问 LM5177是否能够满足输出电压(5-48V)要求。 输出电流(5A)、输出电压(240W)要求和输入电压可以是直流电、但电压范围未受限制? 额定输出功率为5V/3A、9V/3A、15V/3A、20V/3A、20V/5A、 28V/5A、36V/5A 和48V/5A、以满足 PD3.1规范要求。 此外、如果可能、您能否帮助分享如何识别具有不同额定电流的直流/直流输出电压范围?  

谢谢!

迪伦