This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS61021A:0.5V&lt 时 Iq,;VIN<1.8V

Guru**** 2513185 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/999625/tps61021a-iq-when-0-5v-vin-1-8v

器件型号:TPS61021A

你(们)好

在数据表中、Iq = 0.3uA、但 IC 已启用、无负载、无开关 Vin = 1.8V 至3.6V

电压为0.5V <VIN<1.8,what is the IQ? 时 是否有任何测试数据?

现在、我们测试当输入电压=0.58V 时、Iq 为50mA、 输出电压=3.8V、无负载

谢谢!