This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ24075:bq24075

Guru**** 2504515 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/966282/bq24075-bq24075

器件型号:BQ24075

EN1 -0V、EN2 -5V、TS - 0.6V、-ILIM 1K 我的库存中只有1K 而不是1.1K、R-ISET 866 Ω、\

我想以1A 的电流为电池充电、因为我使用的是2500mah、3.7V、我只想在2.5小时内为电池充电。

输入由直流电源提供输入电压:5V

我的问题是直流电源的电流消耗从未超过0.2A、而此电流电池耗时几乎要6小时。  从3V 到3.8V (甚至不是电池的满容量)充电。如何将快速充电电流设置为1A、以便在 不 降低效率的情况下、我的电池能够以2.5A 的电流充电。

谢谢、此致、

P.Akhil