This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ25606:BQ25606问题

Guru**** 2382480 points
Other Parts Discussed in Thread: BQ25606
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/965259/bq25606-bq25606-issue

器件型号:BQ25606

3. ICHG 电阻变为电阻为3.1V 的470电池指示灯,而使用3.43.8V 电池进行测试的5V 侧的1A 电流指示灯正常。 电流设置为2.5A、电池电压现在为3.4V。当电池在正常条件下未放电时、输出为正常的4.2V、并且当负载增加时、不起作用。。