Other Parts Discussed in Thread: TPS82085
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS82085 是否有关于在输入电压= 3.3V、输出电压=-1.3V、输出电流= 1.2A 时将 TPS82085作为 IBB 运行的问题?
对我来说似乎还可以、询问客户... 谢谢!
Steve
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、Steve、
是的、这应该起作用、因为3.3V + 1.3V 低于器件的6Vin 额定值。
以下是类似器件的基本电路的外观: https://www.ti.com/tool/TIDA-01405