This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS92511EVM:该组件是否可以提供12 VDC?

Guru**** 2561600 points
Other Parts Discussed in Thread: TPS92511

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/883223/tps92511evm-can-this-component-be-supplied-with-12-vdc

器件型号:TPS92511EVM
主题中讨论的其他器件:TPS92511

您好!

数据表显示此组件可提供48V 直流电压,但 TPS92511通常接受4.5V 至6.5V 的电压。如果我没有连接12个 LED 的分支,而是连接不到3个 LED (1、2或3),我能否为该组件提供12V 直流电压?

谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Victor:

    只要 LED 总电压低于您的输入电压、只要输入电压高于4.5V、它就能正常工作

    在您的情况下、可通过12V 输入驱动3个串联 LED (大约10V)。