请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28070 大家好、
根据数据表,“这些8-QVFF 电平是为适应85至265VRMS 的完整通用线路范围而设置的。”
如果我们在65V 至265VRMS (最小输入电压低于85VRMS)的输入电压范围内使用 UCC28070、有何问题?
此致、
隐藏
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.