This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS61161:TPS61161的电感器规格审查

Guru**** 2518400 points
Other Parts Discussed in Thread: TPS61161

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/880933/tps61161-inductor-specification-review-for-the-tps61161

器件型号:TPS61161

您好、Sirs、

电感器 P/N F2012HIF-100MT01 (10UH)是否满足 TPS61161的要求、以支持5V 输入电压、3个串联 LED、20mA 峰值电流?
我们可以  根据需要将 FHI2012F-100MT01的数据表发送到产品线。

电感器的简要规格为10uH +/-10%、在60mV、1MHz、125mA 额定电流、0.5ohm DCR、 30MHz SRF。

谢谢、此致、

陈耀恩
2020年2月17日