请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP8556 我们能否在 LP8556中使用不同数量的 LED?
示例:
LED1:7个 LED
LED2:8个 LED
LED3-6:禁用
LED VF = 2V
LED 电流= 50mA/灯串
此致、
标记
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.