This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] UCC28180:UCC28180的应用

Guru**** 2399305 points
Other Parts Discussed in Thread: UCC28180

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/873467/ucc28180-the-application-of-ucc28180

器件型号:UCC28180

根据描述、UCC28180是一款灵活且易于使用的8引脚有源功率因数校正(PFC)控制器、此控制器运行在连续导通模式(CCM)下、以实现交流-直流前端中升压预稳压器的高功率因数、低电流失真和出色的电压调节。

但我想知道 它是否适合 以下情况。

输入电压为32V-80VDC、输出为82VDC、全功率为120W、电流调试结果显示无法在完整输入 范围内稳定、因此这意味 着 UCC28180不适合  应用环境?