Other Parts Discussed in Thread: LM73605
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMR33630 主题中讨论的其他器件:LM73605
尊敬的专家:
我的客户正在寻找具有 LMR33630ADDAR 的引脚对引脚器件、需要实现>60V 的输入电压、IO=2A、Vout=4.3A。 请帮您推荐。 谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.