This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM46000-Q1:评估满足生命要求的物料

Guru**** 2387080 points
Other Parts Discussed in Thread: SN6501-Q1
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/957718/lm46000-q1-evaluate-materials-to-meet-life-requirements

器件型号:LM46000-Q1
主题中讨论的其他器件:SN6501-Q1

℃℃储能项目的寿命要求,工作条件下高温工作试验的等效持续时间应高于105 μ s、10701h 或125 μ s、5508h (可以满足)

2.请帮助评估材料是否符合使用寿命要求。 如果不是、风险点是什么

LM46000QPWPRQ1、

LM46000QPWPTQ1

SN6501-Q1

TCAN1051VDRQ1

TPS76350QDBVRQ1