请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5143-Q1 我需要设计一个输入电压介于48V 至36V@27A 之间的直流/直流转换器。
此外、还能够使用跳线将此设计切换、从而在电流为22安培时从48V 输入电压更改为24V 输出电压
这是否可以使用单路输出四相中的2个 LM5143-Q1器件实现?
如果不是、我可以使用6相还是8相来组合更多的这些芯片吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、Craig、
27A 输出需要2相或4相(取决于 FSW)。 查看应用手册 snva870中的四相设计。
此致、
Tim