请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25895 主题中讨论的其他器件: BQ21120
您好!
我们已启用 BATFET_DLY、然后设置 BATFET_DIS=1。
如果我们在10秒延迟到来之前插入适配器、是否会清除 BATFET_DIS、然后不会进入运输模式?
2.如果在10s 延迟到来之前重置 BATFET_DIS=0、是否会进入运输模式?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.