请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61169 您好!
我是否可以将 TPS61169用于 以下规格、
- VIN= 5V
- VOUT (max)= 15.2V
- Iout (max)= 100mA
- CCM
另请使用 TPS61169为该设计建议电感值。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.