请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24295 CC 充电的下限电流为512mA (REG02.ICHG)、但它是否可以通过将输入电流限制设置为 REG00.IINLIM = 0b001来达到150mA?
还是在 IC 内部放大并保持512mA 的下限?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC 充电的下限电流为512mA (REG02.ICHG)、但它是否可以通过将输入电流限制设置为 REG00.IINLIM = 0b001来达到150mA?
还是在 IC 内部放大并保持512mA 的下限?