This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ25703A:关于电路验证

Guru**** 2771175 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/920363/bq25703a-regarding-the-circuit-verification

器件型号:BQ25703A

我连接了不带主器件和的电路  

要求:

适配器输入:15V/2.4A。

电池额定值:11.1/6.4A。

充电速率为12.6V/1.240A (电池有6节电池、其中电池以串联和并联网络的形式排列、可实现3节电池。每节电池的额定值为3.67V/3.1A)。

如果需要进行任何更改、您能提供帮助吗?

e2e.ti.com/.../1220.Schematic_5F00_ganesha_5F00_2020_2D00_07_2D00_06_5F00_17_2D00_16_2D00_07-_2800_1_2900_.pdf