Other Parts Discussed in Thread: TPS54201
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS54201 大家好、
我的客户对输入电压低于10.8~13.2V、3系列 LED (每个 LED 压降为3.1v、总电压为9.3v)、电流为1.5A 有一个新要求。
TPS54201是否适合在此处使用? 尤其是热压降和电压降。
如果没有、请推荐其他器件。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.