This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS22990:TPS22990:是否有最大 CT (pF)/输出上升时间规格?

Guru**** 2521920 points
Other Parts Discussed in Thread: TPS22990

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/774419/tps22990-tps22990-is-there-a-maximum-ct-pf-output-rise-time-spec

器件型号:TPS22990

我的设置:

TPS22990

输入电压5V

VBIAS 5V

上的电压

0.47 μ F 的 CT

Cin 1.0 μ F

COUT 0.1uF

CLoad ~ 300uF

t RISE 是在1ms 测量的、我预计至少15ms。 在这些电压和负载条件下,开关是否能够上升15ms T?

谢谢