This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 直流/直流转换器 IC

Guru**** 2769425 points

Other Parts Discussed in Thread: LMR33630, LM73606, TPS40210, LM25118

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/797743/dc-dc-converter-ic

主题中讨论的其他器件:LMR33630LM73606TPS40210LM25118

是否有任何 TI IC 可以接受9-36V 输入并提供5V 和12。 单个 IC 同时提供5V 和12V 电压并非强制性要求。 提供5V 输出的 IC 应至少提供6A 电流、而12V IC 应提供2或3A 电流。 上述规范中是否有任何 EMI EA 55032 A 类和 FCC A 级认证?