Other Parts Discussed in Thread: LM2596
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM2596 大家好、下午好
需要实现一个解决方案、该解决方案可从12V 或24V 输入电压输出5V (1.5安培)和12V (2.5安培)电流。
是否有任何具有双路输出的 LM2596或类似器件?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.