请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC2897A 主题中讨论的其他器件:UCC2897
大家好、
UCC2897该芯片的电源输出为12V、上电时会产生大量纹波。
通道1是直流12V 输入:
SS 引脚的波形:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.