Other Parts Discussed in Thread: BQ34110
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ34110 尊敬的所有:
BQ34110的寄存器和功能太多。 TI 是否提供驱动程序软件库?只想加快开发过程。
此电池组为18650锂电池、6系列5并联、单核2800mAH、总容量14AH、最大工作电流20A、充电电流2A。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.