请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC25600 主题中讨论的其他器件:UCC2801、
我的空间不大。
就像我的旧转换器(Ucc2801或类似转换器):
只需将高值电阻器连接至400V -为 Vcc 电容器充电、然后在几毫秒内、该 Vcc 电容器为 UCC25600提供能量、然后偏置绕组开始。
可能吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.