请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2553D 主题中讨论的其他器件:TPS2551
尊敬的先生:
我需要一个限制20mA ~100mA 且 Vdd=2.5V~4.7V 的小型可调节限流器。
你有什么建议吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.