Other Parts Discussed in Thread: TPS53015
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS53015 您好!
我计划使用 TPS53015获得5V 8A 输出、输入电压范围为5V 至17V。
您能否确认 TPS53015是否符合我的要求
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.