请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:PMP22087你(们)好
我计划使用 PMP22087、但没有看到变压器的具体细节、请向我发送包含变压器信息的物料清单。 490µH 90µH 图中的器件型号为750317258、其中 Lm=8 Ω LR=8 Ω
感谢您为具有80 PLUS 铂金兼容性能参考设计的336W 无辅助交流/直流电源参考设计提供帮助。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Wurth 在以下链接中提供了变压器规格:
https://katalog.we-online.com/icref/datasheet/750317258.pdf
此致、
Sheng-Yang Yu