请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25601D 主题中讨论的其他器件:BQ25601、 BQ25606
尊敬的 TI 团队:
请帮助我们检查 BQ25601的默认 OVP 是否为14V、我的输入是否为12V。 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.