Other Parts Discussed in Thread: TPS2052, TPS2052B, TPS2066, TPS2062
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2052 主题中讨论的其他器件: 、TPS2066、 TPS2062
你(们)好
我们在其中一个设计中使用 TPS2052。 数据表中的持续负载电流为500mA、我们能否 持续将该器件加载到1A。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.