请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25703A 在我的应用中,bq25703a 的电源为12V,而电池为12V。
对于配置、我如何执行它的电池单元数量
我选择3S (VCELL_BATPRESZ= 55% VDDA) ?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.