This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS62420:计算反馈电阻器

Guru**** 2524460 points
Other Parts Discussed in Thread: TPS62420

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/793882/tps62420-calculation-of-feedback-resistors

器件型号:TPS62420

您好!

我使用 TPS62420将5V 转换为2.5V/0.19A

我使用图14作为参考。

我计算出 R21=887K Ω、R22=280K Ω。

我还注意到第21页的建议、即两个电阻器应该大约为1Mohm。

在我的案例中、它大约是1.16Mohm..

我还注意到、在下面图14的示例中、两个电阻器之和为1.045Mohm

1.使用这些电流电阻值是否安全?

2.您能解释一下数据表上的1Mohm 限制吗?

此致、