请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM5143你好
以下是客户要求。 我们是否有合适的解决方案、占空比是否为100% POL 解决方案? 谢谢你。
输入电压范围= 5~24V
输出电压/电流= 5V/3A 和3.3V/8A
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.