Other Parts Discussed in Thread: PMP8803
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS23753A 主题中讨论的其他器件:PMP8803
您好!
在 PMP8803 REV A 的原理图中、1A 时的输出为12V、但页面标题为"低成本10W POE 转换器"。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.