请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC29002 主题中讨论的其他器件: UCC39002
我无法完全理解下面突出显示的段落、该段落来自数据表
具体而言、UCC29002是否在 UCC39002中包含逻辑电路、在此逻辑电路中、测得的电流必须超过80%才能启用负载共享?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.