请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5166 大家好、团队、
我想向您核实、如果输出设置为5V、输入较低(例如4.2V)会发生什么情况。
器件是否会进入100%占空比?
谢谢!
垫
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、团队、
我想向您核实、如果输出设置为5V、输入较低(例如4.2V)会发生什么情况。
器件是否会进入100%占空比?
谢谢!
垫
您好!
是的、器件将进入数据表第20页中规定的100%占空比
https://www.ti.com/lit/ds/symlink/lm5166.pdf#page=20
谢谢
-Arief