This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM5022:LM5022:PMP20551参考设计 T1

Guru**** 2515415 points
Other Parts Discussed in Thread: LMV431

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/833764/lm5022-lm5022-pmp20551-reference-design-t1

器件型号:LM5022
主题中讨论的其他器件:LMV431

您好!

Würth 设计(w*ww.ti.com/.../tidrqf9.pdf)中有 T Ü V 的 T1 (750316708)。

截取率 pri 与秒之间的比率为3:1。

输入电压:12至60V。

次级绕组由12V 定义。 因此、如果输入电压为60V、则次级侧的电压为20V。 这是否是故障?
如果次级侧需要48V 电压、Vin 侧需要24V 电压、初级绕组1与次级绕组是否需要1:2的比率?

此致