请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5008 主题中讨论的其他器件:LM5163、 TL783、 TPS7A4001
尊敬的先生:
您能不能推荐任何具有最大输入电压100V 和输出电压12V/200mA 或更高输出电流的线性稳压器。
工作温度范围为-40度至125度。
谢谢、此致、
Nesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.