This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM25088:负压回路

Guru**** 2502205 points
Other Parts Discussed in Thread: LM25088

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/868547/lm25088-negative-pressure-circuit

器件型号:LM25088

我在 TI 的4K 电流计参考电路中看到了12V 输入和-12V 输出电路。
使用的 DCDC 是 LM25088。 我将考虑在未来降低成本、
可能需要使用输出电流小于0.2A 的直流/直流转换器替换 LM25088。

我是否可以将 LM25088替换为输入电压高于24V 的任何降压直流/直流转换器?